Hi, I am implementing MCAN interrupts using MPC5777C_MCAL4_0_RTM_HF4_1_0_1 in MPC5775B.
However, I find the vectors for MCAN module range from 688 to 695, which is beyond the INTC range(vector0~vector511). And it says these MCAN vectors are for Cortex M4 core in MCAN_IM.
So what are the correct interrupt vectors for MCAN in MPC5775B?
Thanks a lot!
Hi,
as per the MPC5777E RM (https://www.nxp.com/docs/en/reference-manual/MPC5775ERM.pdf) the vector number is 348
BR, Petr
Thanks Petr! There are definitely errors in MCAL manual.