WdgIf.xdm in MCAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WdgIf.xdm in MCAL

1,221 Views
Vasily_Wu
Contributor III

Hello,

 When I am choosing WdgIf into EB Tresos, it reports errors, like:

Module "WdgIf_TS_T2D19M10I1R0" (defined in plugin "WdgIf_TS_T2D19M10I1R0") defines the schema file "config/WdgIf.xdm" which cannot be found (if the file is signed or crypted, it must be referenced in META-INF\CRYPTOMANIFEST.MF).

The MCU is MPC5674F.

捕获.PNG

Tags (1)
0 Kudos
Reply
2 Replies

1,215 Views
hungnguyenphi
NXP Employee
NXP Employee

Dear @Vasily_Wu 

 

The WdgIf is just a stub module in the MCAL package. We cannot configure it with EB. 

The WdgIf is provided by third-party(Eg: Elektrobit, Vector,....)

 

Best regards,

Hung

0 Kudos
Reply

1,211 Views
Vasily_Wu
Contributor III

Dear Hung,

Thank you.

0 Kudos
Reply