Warning: Device is not detected or may be censored (MPC5777c)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Warning: Device is not detected or may be censored (MPC5777c)

跳至解决方案
951 次查看
InhyeokHwang
Contributor III

I am having problem debugging with MPC5777c using the example code from S32DS PA 2.1. I've checked all related problems and tried everything but couldn't get through with this. Any suggestions solving this problem?

Thank you.

prob1.jpgprob2.jpgprob3.jpgmyboard.jpg멀티링크.jpg

 

0 项奖励
1 解答
851 次查看
InhyeokHwang
Contributor III

Sorry for the late reply,

I finally solved the problem.

The name of my device was Korean therefore the path of my workspace contained Korean. 

I moved my work space under C:\ and it is working now haha

在原帖中查看解决方案

0 项奖励
4 回复数
925 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Have you ever running this board or is this a first attempt?

Do you see both debugger LEDs on?

0 项奖励
922 次查看
InhyeokHwang
Contributor III

It’s the first time running this board and I see both blue and orange light on.

0 项奖励
897 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

This issue has typically something to do with power supply (as you said it is first attempt to use it, I don't expect the device is censored). Please check jumpers whether they are in right position according to used chip version (LDO or SMPS).

Do you have other MPC EVB to check whether your PeMicro debug probe works well? Try to use different USB cable.

Also you could try to remove MCU from socket and return it back to ensure right contact.

You could also try to decrease JTAG frequency to 1MHz:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-PEmicro-Debug-Connecti...

Check your configuration accorging following link:
https://www.pemicro.com/blog/index.cfm?post_id=180

Also check whether you have latest windows drivers for PeMicro device.

0 项奖励
852 次查看
InhyeokHwang
Contributor III

Sorry for the late reply,

I finally solved the problem.

The name of my device was Korean therefore the path of my workspace contained Korean. 

I moved my work space under C:\ and it is working now haha

0 项奖励