VOL of SPC5777CCK3MMO3R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VOL of SPC5777CCK3MMO3R

467 Views
rajat1293
Contributor I

We are using micro SPC5777CCK3MMO3R in HLC project to turn ON and OFF the BJT transistor.

In our analysis with worst case scenario the VOL is 0.2*Vcc. Our Vcc is 3.3V and 5V. With these inputs the VOL is turning ON the BJT transistor. Can you please provide us the VOL we will get with max current pulled from pin GPIO150 of micro that is 0.1mA to 0.5mA.

 

Kindly provide us the solution on urgent basis.

0 Kudos
Reply
1 Reply

455 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

we provide following specification:

for SR pads:

lukaszadrapa_0-1634276297848.png

And for FS pads:

lukaszadrapa_1-1634276329127.png

We can read the specification like this:

At voltage drop 0.8*VDDEx (for logic '1') or 0.2*VDDEx (for logic '0'), the pads are able to source/sink defined current, at least (or more).

Or in opposite way: if we source/sink defined current from a pad, it is guaranteed that the voltage drop will be lower than 0.8*VDDEx (for logic '1') or 0.2*VDDEx (for logic '0') under all operating conditions.

Unfortunately we do not provide partial specification for lower voltage drop, so it should be characterized by customers in their application. But if we are talking about 0.1-0.5mA currents, I can see no problem here, especially if you use full drive strength.

Regards,

Lukas

0 Kudos
Reply