Hello,
i use MPC5777C with S32-studio.
I tried to multiply in an ISR. If i call for example the function MLIB_Mul(FRAC32(0.185), FRAC32(0.195), F32), an IVOR1-exception occurs.
Then i tried the function MLIB_Abs() within this ISR. Its output result is the same as input (negative sign) - not ok.
In any loop, which is called from the main loop, all this functions works fine. Only in any ISR is no function.
Can you give support?
Thank you,
Robert.
Hi,
I'm not AMMCLIB expert, I have just one general idea which sometimes causes troubles:
When IVOR4 is entered, FP and SPE bits in MSR register are automatically cleared. If user wants to use FP or SPE instructions, it must be enabled by the software again. For example:
void SPE_enable(void)
{
mfmsr r3
e_add2is r3,0x0200
mtmsr r3
}
Maybe this could help.
Regards,
Lukas