Hi,
MCU - MPC5777C
IDE- S32DEv1.2
We are using Eqadc-A & Eqadc-B channels for analog to digital conversion.
We are using channels ANA6,ANA34,ANA35,ANA36 etc and able to convert analog data to digital.
Now we are using,
ANB16/GPI484/ETPUC15/EMIOS24
ANB17/GPI485/ETPUC14/EMIOS25
ANB18/GPI486/ETPUC13/EMIOS26
ANB19/GPI487/ETPUC12/EMIOS27
But Unabble to make conversion.
Following is our init code.
EQADC_B.CFPR[0].R = 0x00800301; // configure ADC_CR0 Register in buffer 0
EQADC_B.CFPR[0].R = 0x82800301; // configure ADC_CR1 Register in buffer 1
EQADC_B.CFCR0.R = 0x1C101C10;
EQADC_B.CFCR1.R = 0x1C101C10;
EQADC_B.CFCR2.R = 0x1C101C10;
// Wait for Queue Done
while (EQADC_B.FISR[0].B.EOQFX == 0) { } /* Wait for End Of Queue flag */
EQADC_B.FISR[0].R = End_of_Queue_Flag;
EQADC_B.IDCR0.R = 0x33033303;
EQADC_B.IDCR1.R = 0x33033303;
SIU.PCR[ANB16_TO_ADC_INV2_TA].R = PRIM_F | K_IBE; //ANB16/GPI484/ETPUC15/EMIOS24
SIU.PCR[ANB17_TO_ADC_INV2_TB].R = PRIM_F | K_IBE; // ANB17/GPI485/ETPUC14/EMIOS25
SIU.PCR[ANB18_TO_ADC_INV2_TD].R = PRIM_F | K_IBE; // ANB18/GPI486/ETPUC13/EMIOS26
SIU.PCR[ANB19_TO_ADC_INV2_TC].R = PRIM_F | K_IBE; //ANB19/GPI487/ETPUC12/EMIOS27
Please suggest missing or incorrect part.
Thanks.
Rahul.
Hi, I have just created example code for this configuration.
It works fine on my side. You can download it here:
https://community.nxp.com/docs/DOC-335394
Hope it helps
Hi,
We have tested the code it is working but we are getting sampling frequency =300KHz.
We want to sample the signal having frequency 50KHz.
The samples that we are getting are not sufficient.
We have set peripheral clock frequency == 96MHz
ADC clock == 24MHz
conversion cycles ==2
So sampling frequency should be 1.5MHz. But practically we are getting 300KHz
We have verified it by giving 50KHz signal input. We are getting 8 samples in 1 cycles of waveform.
PUSH_TO_CFIFO1_B ( B0 |
ADC_REG_VALUE (0x8001) | // enables ADC0 0x8001 == divide by 4 //0x8002 == ADC0/1_CLK_PS divide by 6
ADC_REG_ADDR (ADC0_CR) );
LST == 0 // 0 means 2 cycles for conversion.
How to achieve 1.5 MHz sampling frequency?????
Thanks.
Rahul
Thanks.
We will check & update you.
Hi David,
Hi David,
We have not been able to read the adc values using DMA yet.
Can you go through the above snaps of our CQueues.
Thanks.
Rahul