Hello everyone,
it's a couple of days that I'm struggling with a TRK-MPC5634M board and still I can't communicate with it.
I tried both the embedded programmer and an external PE USB multilink without any success.
I tried both USB power and external power (J1 has been changed accordingly).
I checked all the rail on the board and everything is on spec.
When I try the embedded programmer simply I get a red message sayng 'Undetected. Disconnect/Connect USB cable. Click Refresh List (FAQ 29)'.
If I close JC5 (OSJTAG_IRQ) I find the device in bootloader mode.
The driver check utility from PE says that everything is fine.
When I try the external PE USB multilink via JTAG I'm able to find and select it but when I try to connect I get those errors:
-Debugger retrying force to background mode
-Can not enter debug mode
My OS is WIN 7 64bit, CodeWarrior 5.9.0 build 3510 and I'm using the latest driver from PE site.
I'm missing something?
Thank's for any help.
Regards,
FML