Hello,
Here is closer explanation.
best regards,
Peter
Hello,
Here is closer explanation.
best regards,
Peter
Hello,
Hmm, I am confused a bit.
There are Two EQADC modules, each containing two internal ADCs and Four Sigma-Delta (SD) ADC modules.
Each ADC module has its own channels. So I am not sure what the question is here. You cannot measure eQADC channel with SDACD as it is its internal IP separate from SDACD.
But if you are referring to the same pin which you like to measure then only one ADC can be routed to it at the time.
I am not sure what you are trying to achieve, but redundant measurements can be done.
Best regards,
Peter
Hi @petervlna
First of all thank you for your response.
I would like to ask my question in a different way.
There is a photo below. ANA0_SDA0 analog channel has been dedicated for EQADC and SDADC. Can I read data from this channel with EQADC and SDADC at the same time?
I hope, I can explain my question more clearly.
Hello,
Yes, it is possible to read data from that channel with both ADCs but it is not recommended to do so due to sharing of charge. It just not make any sense.
If you need redundant measurement, simply connect same signal on 2 pins and use 2 ADCs. Make sure pins are not close to each other.
Best regards,
Peter