hi
When i use the map file for Mpc5606B, there are some global big data in the .data section of map ,which i can't find in the source file?
just like
00000010 000050 40000010 000af1b0 1 .data exl.o
00000010 000009 40000010 000af1b0 4 exl_SIULCfgTabl exl.o
0000001c 000044 4000001c 000af1bc 4 @604 exl.o
the "@604" is a object in the exl.o, but i can not fine which is?
DO U have any document for this issue ,thks
Hi,
which IDE and which version do you use? What kind of software have you included into your project? I can see nothing like that in my projects.
Regards,
Lukas
Hi,
I was asking around but the only information I got is that it is something like substitute pointer used by compiler. I didn't get a documentation about that.
Regards,
Lukas
Hi
I use the makefile to build, and the tool list is as follow, So the IDE is the CW 2.10.
the
TOOL_PATH = C:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.10
CC = "$(TOOL_PATH)\PowerPC_EABI_Tools\Command_Line_Tools\mwcceppc.exe"
ASMBLER = "$(TOOL_PATH)\PowerPC_EABI_Tools\Command_Line_Tools\mwasmeppc.exe"
LINK = "$(TOOL_PATH)\PowerPC_EABI_Tools\Command_Line_Tools\mwldeppc.exe"