Some PCS pins do not work in DSPI0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some PCS pins do not work in DSPI0

Jump to solution
588 Views
kerem01011
Contributor II

I have two sensor communicate with DSPI0 with two chip select. One chip select works what I expect. But second chip select do not work properly. I think second pin may be crush or something and I change the second chip select's pin. I try four chip select pin for this purpose and I see only first one works. I do not understand why this happen. Is this problem cause for software or hardware I do not know actually. 

First chip select PCSA0(it works):

kerem01011_0-1683705492524.jpeg

Second chip select PCSA1(it does not work; interestingly chip select's reset state around 0.4V (I expect 5V)):

kerem01011_1-1683706061547.jpeg

PCSA2: I do not use this pin because I do not see this pin in my motherboard

PCSA3(this pin does not work): When I select this pin as a second chip select This pin always in low state (0V):

kerem01011_2-1683706603202.jpeg

PCSA4(this pin does not work but it has interesting output): When I select this pin as a second chip select it does not work and generate interesting output:

kerem01011_3-1683706719499.jpeg

PCSA5(it does not work): When I select this pin as a second chip select This pin always in low state (0V):

kerem01011_4-1683706774918.jpeg

 

By the way I use this motherboard: 

kerem01011_5-1683706860621.png

And Which information I use for determine the chip select pins:

mother_board_PCSA1.png

mother_board_PCSA3.png

reference_manual_PCSA_Pins.png

 And lastly I want to share with you what configuration I did about software:

kerem01011_6-1683707127217.png

 

 

0 Kudos
Reply
1 Solution
571 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

They are jumper for ethernet PHY on these pins (routed to motherboard). Check them, whether you have them in place or not.

davidtosenovjan_0-1683805725235.png

 

 

View solution in original post

2 Replies
572 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

They are jumper for ethernet PHY on these pins (routed to motherboard). Check them, whether you have them in place or not.

davidtosenovjan_0-1683805725235.png

 

 

551 Views
kerem01011
Contributor II
Thank you very much, it works for me
0 Kudos
Reply