S32DS MPC5604 BAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS MPC5604 BAM

939 Views
CCandido
Contributor V

Hi, 

my projets with MPC5604, compiling, debug and running flash ok.

how to BAM projects with S32DS ?

questions:

1. how to set addr start programa 0x4000.0000 or 0x4000.0100, and how to set in S32DS ?

   config to code for RAM.

2. when, loader code in ram, jump app automatic ?

thanks,

Carlos.

Labels (1)
Tags (1)
0 Kudos
4 Replies

777 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I described the procedure in this post:

https://community.nxp.com/thread/320166#comment-384300 

Yes, when the image is loaded by BAM to RAM, the image is automatically executed.

Regards,

Lukas

0 Kudos

777 Views
CCandido
Contributor V

Hi Lukas,

thanks your help,

I. tested with CW 5.9.

flash dbug and running ok,

based: https://community.nxp.com/thread/320166#comment-384300 

edit lcf  RAM to 

MEMORY
{
init: org = 0x40000000, len = 0x00001000

pseudo_rom: org = 0x40001000, len = 0x00011000

exception_handlers: org = 0x40012000, len = 0x00001000

internal_ram: org = 0x40013000, len = 0x0000A000

heap: org = 0x4001D000, len = 0x00001000 // Heap starts

stack : org = 0x4001E000, len = 0x00001000 // Start location for Stack
}

SECTIONS
{
GROUP : {

.init_vle (VLECODE) : {

*(.init)

*(.init_vle)

}

.init : {}

} > init  ok

add file __start.c in folder ok

compilinng ok

run debug = not runing !

qustions
run with debug ?

or runing with  BAM ?

see code

thanks,

Carlos

0 Kudos

779 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's 32KB or 48KB of RAM depending on your derivative:

pastedImage_1.png

And I can see that you have updated the linker file in this way:

pastedImage_2.png

This will not work of course, this is out of physical RAM. You can't update the linker file in this way.

Regards,

Lukas

0 Kudos

779 Views
CCandido
Contributor V

Hi Lukas,

I tested with CW, debug in RAM ok,

MEMORY
{
pseudo_rom: org = 0x40000000, len = 0x00003000
init: org = 0x40004000, len = 0x00001000
exception_handlers: org = 0x40005000, len = 0x00001000
internal_ram: org = 0x40006000, len = 0x00001800
heap : org = 0x40007800, len = 0x00000400 /* Heap start */
stack : org = 0x40007C00, len = 0x00000400 /* Stack Start */
}

s19:

S0030000FC
S319400000007C6000A664637C600124000470BF7FF146350653E5
S3194000001404347C00286C00017C002FAC18A5900818849CF86D
S31940000028E0F7000100040000023602470258780000A779FF30
S3194000003CFFC7182106F84800D0012C00D101780000AD706859
S31940000050E0001C6311E00093000570C8E0001CC610000096CE
S31940000064036303740385000570C8E0001CC611F20096000540
S31940000078182106E00080D901D7F1D6E1D5D1013E014D015FA3
S3194000008C2A0FE60C0DDEE60A01E301D401F5780000B901E350
S319400000A001F479FFFF6BC7F1C6E1C5D1C901009021F10004CA
S319400000B4182106D00080DD01DBF1D431014F2A0FE606C4314A
S319400000C8480401F578000137CBF1CD0100901C210030000461
S319400000DC7028E0021C21F0007048E0021C42B00C71A8E00274
S319400000F01DADB0000004182106E00080D901D7F1D6E17108C7
S31940000104E0001FE8022CC00F2A00E207C10F2A00E204C20FF9
S319400001182A00E607C13FC04FC25FE9AB20BFE8F27108E000A0
S3194000012C1FC802BCC00E2A00E204C10E2A00E606C03EC14E04
S31940000140E9BA207EE8F6C7F1C6E1C901009021F100040D3436
S31940000154E40D24041CC3FFFF2005E8058104910620042006E3
S319400001682605E2FBE80E04547CC32A142005E8073104FFFF23
S3194000017C3506FFFF240424062605E2F9000423F57480063F43
S319400001902403E4317C6418F81884C803E6060645910326048D
S319400001A42003E2FD2A00E60B7407402F7406C00F7404801F9A
S319400001B844077CC02378447074A4D97F2A042423E60CD1036C
S319400001CC2604D203D303D403D503D603D703D80321F3E2F6DB
S319400001E074A4F77F2A04E605D10326042033E2FD20232E3548
S319400001F42A05E605910326052003E2FD00040080D101182147
S3194000020806E0D7F1013FE9BE01F3C7F121F1C10100900004F3
S3154000021C70A8E0001CA51334D024D0530004000071
S3194000022C40000000400000000000022C4000022C4000022CEE
S31940000240000000A84001200040012000000001004001210097
S3194000025440012100000000A840001000400010000000029C08
S31940000268400012A0400012A00000000C400012AC400012AC50
S3194000027C00000008400012B4400012B400000008400012BCFE
S31940000290400012BC00000030400012EC400012EC00000088D2
S319400002A440013000400130000000000400000000000000001A
S319400002B8000000004001300800000004400130100000000CE2
S30D400002CC0000000000000000E4
S31940001000182106D00080DD01DBF1DAE1D9D14800D401480F84
S31940001014481E1FAD8008780000D9780001537800009FC4319F
S319400010281C030001D401C4017060E01F1C6384800C30E1192C
S3194000103C1BFFE00177E0063F7138E3F931090644740807FE39
S319400010503509064477E0063F7138E3F931090645740807FE97
S31940001064350906454800D401C03D1C030001D00D62C31C63EE
S31940001078A1200C30E1D51BDEE00177C0063F7138E3F9310956
S3194000108C0646740807FE3509064677C0063F7138E3F9310978
S319400010A00647740807FE350906474800D00DE8BCCBF1CAE16D
S319400010B4C9D1CD0100901C2100300004712002017118E3F980
S319400010C85D2800C8712002017118E3F95D2800CA71200201A5
S319400010DC7118E3F95D2800CC712002017118E3F95D2800CEB8
S319400010F0000449D07118E3FE5408C0087120E2401D29010001
S319400011047118E3FE552800A07120E01F1D2900747118E3FE56
S319400011185528C03049007118E3FE5408C08448107118E3FEFB
S3194000112C3408C1047128E0001D295AF07118E3FE5528C004B4
S319400011407128E0011D29A50F7118E3FE5528C0047118E3FECC
S319400011545108C00075002FFF2A00E2F97118E3FE5008C000FE
S3194000116869C02230E2FA00047120E0011D29C520711FE7F4CA
S3194000117C552880107120E0011D29D928711FE7F455288010DB
S319400011907130E0001D29010A711FE7F455288000000418218E
S319400011A406E00080D9017108E0001C6812A0C043C103D44146
S319400011B8D501C203D6017062E0861C6380ED7098E3F91C84C3
S319400011CC801C1D8100107D8903A60007C901009021F1000459
S319400011E0182106F00080D501E9DDC501009020F100041821C6
S319400011F406F00080D5017800000DC501009020F10004000065
S3194000120870A8E0011CA53010C2052A00E207D0354810D14545
S3194000121C4803D205E8022C0300042A03E20C1803A00C70687F
S31940001230E0011C63301004034800D003D103D2030004C01124
S31940001244C101009000040080D101182106E0510D800073E850
S319400012589FFEE20D1C6100101C81001479FFEFB9C431C54157
S3194000126C79FFFF9D546D800079FFFFCE0080D101182106F00D
S31940001280506D800073E39FFEE60779FFFF9D711F7FFE550D74
S30D40001294800079FFFFAC000069
S311400012A0D03444007C0006AC440000043E
S30D400012AC4000124A0000000058
S30D400012B4400012780000000022
S319400012BC1808000000000000000800000000000008080000A0
S319400012D0000000001808000000000000080800000000000094
S30D400012E41008000000000000A4
S319400012EC40001000000000C0400012BC400121000000000226
S31940001300400012C44001211000000096400012CC400000789F
S319400013140000003C400012D4400000B400000028400012DCD3
S31940001328400000F60000005C400012E4400012EC400012F81B
S3194000133C40001000000000C0400012F8400013104001210038
S31940001350000000A6400013104000133440000078000000DA21
S315400013640000000000000000000000000000000033

delet it parte ok  ?
S31940012000E8004400440044004400440044004400E800440095
S31940012014440044004400440044004400E80044004400440025
S319400120284400440044004400E8004400440044004400440011
S3194001203C44004400780000D0440044004400440044004400E1
S31940012050E8004400440044004400440044004400E800440045
S31940012064440044004400440044004400E800440044004400D5
S319400120784400440044004400E80044004400440044004400C1
S3194001208C44004400E8004400440044004400440044004400AD
S319400120A0E8004400440044004400440044004400E8004400F5
S319400120B4440044004400440044004400E80044004400440085
S319400120C84400440044004400E8004400440044004400440071
S319400120DC44004400E80044004400440044004400440044005D
S315400120F0E8001800D0001800D0001800D0000000F9
S3194001210000080000000000000000000000000000182106A09D
S31940012114D80100A0D4017C0102A6D5017C000026D60100802E
S31940012128D701D931DA41DB51DC61DD71550100385521003C68
S3194001213C55410040556100445581004857E1005C711FE7F55A
S3194001215053E88010519F00007D8903A600074800711FE7F50F
S319400121645408801853E1005CC931CA41CB51CC61CD715101BE
S3194001217800385121003C514100405161004451810048C4017F
S3194001218C00B0C5017C0103A6C6017C0FF120C7010090C801D8
S30D400121A01C210060000800004B
S30940013000FFFFFFFE8A
S705400000308A

and convert S19 to bin ok, pleace code

now preparing send file BAM CAN mode ( DLC = 8 ever).

thanks,

Carlos

0 Kudos