CodeWarrio is V11.0 But
When debugging with Flash, the brake works, but
When debugging with RAM, the brake does not work
And if you turn off the power of the EVB board and turn it on again, all the firmware on the board disappears.
Do you know why?
Hi,
which version of CodeWarrior do you use?
Regards,
Lukas
CodeWarrio is V11.0 But
When debugging with Flash, the Break point works, but
When debugging with RAM, the Break point does not work
And if you turn off the power of the EVB board and turn it on again, all the firmware on the board disappears.
Do you know why?
Isn't that something similar to this topic?
And there's nice article from Erich Styger:
https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/
If you have RAM project then yes, it will disappear after power off-on sequence. But if you have flash project, it will definitely stay in flash. There's no reason for erase.
Regards,
Lukas