MPC5xxx, Internal Flash Erase/Write a Privileged operation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5xxx, Internal Flash Erase/Write a Privileged operation?

780件の閲覧回数
richarddavis
Contributor I

We are developing a boot utility for loading internal Flash with a MPC5554.  Our Flash Programming utilities are working as long as the processor is running in Privilege Mode (MSR.PR = 0).  But, if we switch to User Mode (MSR.PR = 1) the processor crashes (exceptions and finally a reset).  Indications are that things begin going wrong when either the Erase or Write functions start to write to the Flash registers:

  • Flash_MCR (16 #C3F8_8000#)
  • Flash_HLR (16 #C3F8_8000#)
  • Flash_HSR (16 #C3F8_8000#)

Our debug environment is not particularly reliable when the processor is in User Mode so I hesitate to get into the details of the failure.  Depending on my test code I have seen Machine Check and Program-Privilege Exceptions.  But, they might not have been the first exception.

 

I am concerned that the Flash Register memory space (C3F8xxxx) is considered a “privileged resource”.  This would not surprise me considering what the registers control.  But, I did not find anything in the documentation that specifically said it.   Can anyone confirm this is/isn’t the case?

 

If it helps we are using the following definition for the TLB for that memory space:

 

MAS1

 

reserved-0

0 (0x0)

Selected TLB (must be 1)

TLBSEL_ (0x1)

reserved-0

0 (0x0)

Enytry select for TLB1

ESEL_ (0x0)

reserved-0

0 (0x0)

Next replacement victim

NV_ (0x0)

MAS2

 

Valid

VALID_Y (0x1)

Invalidation protect

IPROT_Y (0x1)

reserved-0

0 (0x0)

Translation ID

TID_ (0x0)

reserved-0

0 (0x0)

Translation Address space

TS_ (0x0)

Entry page size

TSIZE_1M (0x5)

reserved-0

0 (0x0)

MAS3

 

Effective page number

0x0C3F00

reserved-0

0 (0x0)

Write Through

W_N (0x0)

Cache Inhibited

I_Y (0x1)

Memory coherence (ignored)

M_N (0x0)

Guarded (ignored)

G_Y (0x1)

Little Endian

E_N (0x0)

MAS4

 

Real Page Number

0x0C3F00

reserved-0

0 (0x0)

User bit 0

U0_N (0x0)

User bit 1

U1_N (0x0)

User bit 2

U2_N (0x0)

User bit 3

U3_N (0x0)

User Execute

UX_Y (0x1)

Supervisor Execute

SX_Y (0x1)

User Write

UW_Y (0x1)

Supervisor Write

SW_Y (0x1)

User Read

UR_Y (0x1)

Supervisor Read

SR_Y (0x1)

 

 

  

Any assistance would be appreciated.  If you can point me to the area of the documentation that supports your ideas, that would be really appreciated. 

1 返信

607件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't think flash registers would require supervisor mode, but if you default setting of PBRIDGE, it requires such access for flash registers. Pay attention to screenshots below:

pastedImage_2.png

pastedImage_3.png

Hope it helps