Re: ADC External Channels Usage in MPC746C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: ADC External Channels Usage in MPC746C

565 Views
kavithakakarla
Contributor II

Thanks for the explanation.

To be more clear Iam looking for the below details:

For example Assume, ADC0_X[0] (external channels 64 to 71 of MPC5764C) is been connected to an external 8:1 MUX and ADC0_MA[0] to ADC0_MA[2] are configured for the select lines. And the ADC0_CTR2 register is updated to enable normal conversion for the channels 64 to 71.

And now if the ADC0_MA[0] to ADC0_MA[2] is been updated to select the ADC Channel 67, and the normal conversion is started with ADC0_MCR[NSTART]=1. 

Will the ADC converts all the channels from 64 to 71 (since all these channels are enabled for Normal Conversion with ADC0_CTR2 register)

OR

Only the channel 67 will be converted since the select lines for external MUX are configured to output only Channel 67.

0 Kudos
1 Reply

443 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It converts all channels in sequence, it is the same as as with normal channels.

0 Kudos