MPC5777M pinout information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M pinout information

Jump to solution
3,003 Views
jschloss
Contributor III

Hi,

Can somone point me to the pinout /signal information for the MPC5777M? For the 77C i found it attached to the reference manual, but for the 77M the reference manual says "refer to the MPC5777M Microcontroller Data Sheet" and the datasheet says "See the MPC5777M Microcontroller Reference Manual for signal information." I'm trying to find the mapping for GPIO registers in the SIUL2 to physical pins.

Thanks,

Jacob

Tags (1)
1 Solution
2,290 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, now I see the issue.

In latest RM rev 4.3 there is not attached excel with IO signals definition.

Strange, as it was normally attached in previous versions.

However I will post it here so you can download it.

Peter

View solution in original post

7 Replies
2,291 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, now I see the issue.

In latest RM rev 4.3 there is not attached excel with IO signals definition.

Strange, as it was normally attached in previous versions.

However I will post it here so you can download it.

Peter

2,290 Views
fraidling
Contributor II

This is a helpful and clear overview of the I/O Signals! 
Is there an equivalent Excel Sheet for the MPC5777C?

0 Kudos
Reply
2,290 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

yes this is attached to reference manual.

But just in case I will post it also here.

Peter

2,290 Views
johnmitchell
Contributor I

Thank you for posting this. I searched MPC5777CRM.pdf (all 3375 pages of it) looking for keywords like: 'system_io_definition', 'attachment', 'pinout', 'xlsx'  etc, etc, but the only hits were on text saying the attachment was there, but no links and the attachment itself I couldn't find. They've hidden it really well !!! Thanks !

0 Kudos
Reply
2,290 Views
petervlna
NXP TechSupport
NXP TechSupport

Well, the IO spreadsheet is embedded attachment in pdf.

Looks like you hear it first time, so here is example how it looks in MPC5777C ref manual:

pastedImage_1.png

Embedded attachments are usually in pdf viewers represented by paperclip.

Peter

0 Kudos
Reply
2,290 Views
johnmitchell
Contributor I

Thank you. It isn’t quite as obvious in Acrobat reader, but the paperclip icon is there and now I know what it means ! (I’d been looking for a link in the document itself). Thanks.

John Mitchell | Senior Electronic Design Engineer | McLaren Applied Technologies

McLaren Technology Centre (G+1), Chertsey Road, Woking, Surrey GU21 4YH, UK

T +44 (0) 1483 261487

E john.mitchell@mclaren.com<mailto:firstname.lastname@mclaren.com>

W www.mclaren.com/appliedtechnologies/<http://www.mclaren.com/appliedtechnologies/>;

0 Kudos
Reply
2,290 Views
jschloss
Contributor III

Thank you!

0 Kudos
Reply