MPC5777M flexray startup fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M flexray startup fails

1,230 Views
bwp530
Contributor IV

I want to test flexray communication on MPC5777M EVB. So I take the flexray-channel A on board as channel A of FR_0 and take flexray-channel B as channel A of FR_1 by connecting J30 to PN[12] PN[14] PN[6]. FR_0 and FR_1 only work for single channel mode. I connect channel A of FR_0 to channel A of FR_1. 

1.png

when i test the flexy communition like this, flexray startup fails:

1. CSA_IF in PIFR0 is set;

2. CSAA in PSR1 is set;

3. STARTUPSTATE in PSR0 is 5 (POC:integration listen)

my configurations are:

#define gdActionPointOffset 3
#define gdStaticSlot 50
#define gdMinislot 40
#define gNumberOfStaticSlots_1 60
#define gColdstartAttempts 28
#define gdMinislotActionPointOffset 3
#define gdWakeupSymbolRxLow 50
#define gdCASRxLowMax 83u
#define gdWakeupSymbolRxWindow 301u
#define gdTSSTransmitter 11
#define gdWakeupSymbolRxIdle 59
#define gdWakeupSymbolTxLow 60
#define gdSymbolWindow 13
#define pMacroInitialOffsetA 5
#define pMicroPerMacroNom 40
#define pDecodingCorrection 56
#define gdWakeupSymbolTxIdle 180
#define gMaxWithoutClockCorrectionFatal 14
#define gMaxWithoutClockCorrectionPassive 10
#define gNumberOfMinislotsEnable 1
#define gdSymbolWindowEnable 1
#define pOffsetCorrectionOut 1201
#define gMacroPerCycle 5000
#define pSingleSlotEnabled 1
#define pWakeupChannel 0
#define gOffsetCorrectionStart 4920//(gMacroPerCycle - adOffsetCorrection)
#define pKeySlotUsedForStartup 1
#define pKeySlotUsedForSync 1
#define pAllowPassiveToActive 20
#define headerCRCForKeySlot 242


#define pRateCorrectionOut 600
#define pMacroInitialOffsetB 5
#define pKeySlotId 1
#define pWakeupPattern 16
#define gPayloadLengthStatic 16
#define pDecodingCorrection 56
#define pMicroInitialOffsetA 23
#define pMicroInitialOffsetB 23
#define pLatestTx 21
#define pExternRateCorrection 0
#define pdAcceptedStartupRange 300
#define pDelayCompensationA 1
#define pPayloadLengthDynMax 8
#define pClusterDriftDamping 1
#define pAllowHaltDueToClock 0
#define pdAcceptedStartupRange 300
#define pDelayCompensationB 1
#define gdDynamicSlotIdlePhase 0

#define gNumberOfMinislots 22
#define pExternOffsetCorrection 0
#define gSyncNodeMax 5
#define pdListenTimeout 401202
#define gListenNoise 2
#define pMicroPerCycle 200000
#define pdMaxDrift 601

#define gNetworkManagementVectorLength 2

I try to change flexray clock to 40Hz frim 80Hz, but it does't work. PetrS b55689

Labels (1)
2 Replies

997 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

because of Flexray module complexity, this is not directly supported.

If you want to have Flexray support, please contact sales representative for your area or use NXP professional services.

Distributor Network | NXP 

Professional Services Software Technology | NXP 

Thank you for understanding.

Regards,

Martin

997 Views
Deepak1
Contributor IV

Hi,

I want to understand how to calculate configuration parameters for nodes in flexray.

Above it is calculated as,

#define gdActionPointOffset                     3
#define gdStaticSlot                               50
#define gdMinislot                                  40
#define gNumberOfStaticSlots_1         60
#define gColdstartAttempts                  28
#define gdMinislotActionPointOffset     3
#define gdWakeupSymbolRxLow         50

0 Kudos