MPC5777C FlexCan RX FIFO filtering

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5777C FlexCan RX FIFO filtering

跳至解决方案
2,711 次查看
darq
Contributor III

Hello,

When RX FIFO is enabled, by default MB0-5 are used for the FIFO and MB6-7 are used for the filters for FIFO (CAN_CTRL2[RFFN] = 0 means 8 entries for filters). When i add one entry of the filter lets say 0x100 it works ok, but i can also see that frames with ID 0 are accepted into the FIFO because i assume other entries are empty. What is the proper way to filter out those frames? I don't really like idea of filling all filter entries with the same ID because i would like to leave them for future extensions. Or am i misunderstanding something?

Best regards

0 项奖励
回复
1 解答
2,684 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

whole filter ID table is used for matching algorithm, so you should initialize whole ID table. 
The ID is accepted by RXFIFO based on this ID table and acceptance mask registers. So if you have rest of filter elements cleared and mask registers set to compare all bits of IDs, then ID 0 will be accepted by RXFIFO too, simply because there is matched ID in the filter table
Thus the only way is to fill all entries with the same ID as you wrote. But you can easily update filter table based on your needs in future.

BR, Petr 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,685 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

whole filter ID table is used for matching algorithm, so you should initialize whole ID table. 
The ID is accepted by RXFIFO based on this ID table and acceptance mask registers. So if you have rest of filter elements cleared and mask registers set to compare all bits of IDs, then ID 0 will be accepted by RXFIFO too, simply because there is matched ID in the filter table
Thus the only way is to fill all entries with the same ID as you wrote. But you can easily update filter table based on your needs in future.

BR, Petr 

0 项奖励
回复