MPC5777C CSE Boot MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C CSE Boot MAC

Jump to solution
1,759 Views
jeffcampbell
Contributor III

Quick question on the CSE - in the manual in the section for Secure Boot, it say that the MAC calculated over the secure boot region is compared with the stored BOOT_MAC, and if the stored value is zero, the new MAC is stored there instead.  If the secure boot section were to be modified at some point, is it possible to overwrite the value stored in BOOT_MAC?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,501 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to change the BOOT_MAC if secure boot section needs to be modified. But this assumes some conditions and there can be different scenarios. Please refer to the CSE App Note "AN4234-Using CSE" for detailed description. Particularly refer the "Section 2.10: Code flash update procedure" which discusses this question. There are also SW examples for this App Note. Please see example "D.1.2: Reprogramming of a programmed part".

Peter

View solution in original post

0 Kudos
Reply
2 Replies
1,502 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to change the BOOT_MAC if secure boot section needs to be modified. But this assumes some conditions and there can be different scenarios. Please refer to the CSE App Note "AN4234-Using CSE" for detailed description. Particularly refer the "Section 2.10: Code flash update procedure" which discusses this question. There are also SW examples for this App Note. Please see example "D.1.2: Reprogramming of a programmed part".

Peter

0 Kudos
Reply
1,501 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have spoken to application team and looks like we need to ask design directly.

I will inform you as soon as I will get reply from design.

Peter

0 Kudos
Reply