My init code :
void sdADC_Init()
{
sdadc_init(Mcal_SDADC_OSR_24, Mcal_SDADC_Gain_2, Mcal_SDADC_FTHLD_8, Mcal_SDADC_DIFF);
}
void sdadc_init(uint8_t pdr, uint8_t gain, uint8_t fifo_thld, uint8_t inp_mode)
{
/*####################################
* SD ADC 1 CONFIGURATION
####################################*/
SDADC_1.SFR.R = 0x1B; // clear all the status flags
SDADC_1.FCR.B.FRST = 1; // generate reset to flush FIFO
SDADC_1.FCR.B.FTHLD = fifo_thld; // FIFO threshold - overcome generates FIFO full event flag
SDADC_1.FCR.B.FSIZE = 3; // FIFO size: 0 - 1 word, 1 - 4 words, 2 - 8 words, 3 - 16 words
SDADC_1.FCR.B.FOWEN = 0; // disable FIFO overwrite
SDADC_1.FCR.B.FE = 1; // enable FIFO
SDADC_1.RSER.B.DFFDIRS = 1; // DMA request on data FIFO full
SDADC_1.RSER.B.DFFDIRE = 1; // data FIFO full request enable
SDADC_1.MCR.B.MODE = inp_mode; // input mode: 0 - differential, 1 - single-ended
SDADC_1.MCR.B.PDR = pdr; // Oversampling rate
SDADC_1.MCR.B.PGAN = gain; // Gain
SDADC_1.MCR.B.HPFEN = 1; // High-pass filter enabled
SDADC_1.MCR.B.EN = 1; // internal SDADC modulator enabled
SDADC_1.OSDR.B.OSD = 1; // set the output settling delay
SDADC_1.CSR.B.ANCHSEL = 0; // analog input channel AN[x] selection
SDADC_1.MCR.B.TRIGEN = 1; // enable HW trigger
/*####################################
* SD ADC 2 CONFIGURATION
####################################*/
SDADC_2.SFR.R = 0x1B; // clear all the status flags
SDADC_2.FCR.B.FRST = 1; // generate reset to flush FIFO
SDADC_2.FCR.B.FTHLD = fifo_thld; // FIFO threshold - overcome generates FIFO full event flag
SDADC_2.FCR.B.FSIZE = 3; // FIFO size: 0 - 1 word, 1 - 4 words, 2 - 8 words, 3 - 16 words
SDADC_2.FCR.B.FOWEN = 0; // disable FIFO overwrite
SDADC_2.FCR.B.FE = 1; // enable FIFO
// DMA settings
SDADC_2.RSER.B.DFFDIRS = 1; // DMA request on data FIFO full
SDADC_2.RSER.B.DFFDIRE = 1; // data FIFO full request enable
SDADC_2.MCR.B.MODE = inp_mode; // input mode: 0 - differential, 1 - single-ended
SDADC_2.MCR.B.PDR = pdr; // Oversampling rate
SDADC_2.MCR.B.PGAN = gain; // Gain
SDADC_2.MCR.B.HPFEN = 1; // High-pass filter enabled
SDADC_2.MCR.B.EN = 1; // internal SDADC modulator enabled
SDADC_2.OSDR.B.OSD = 1; // set the output settling delay
SDADC_2.CSR.B.ANCHSEL = 0; // analogue input channel AN[x] selection
SDADC_2.MCR.B.TRIGSEL = 0; // SDADC_1 trigger output selected as an input trigger for SDADC
SDADC_2.MCR.B.TRIGEDSEL = 1; // rising edge of trigger input selected
SDADC_2.MCR.B.TRIGEN = 1; // enable HW trigger
}
void sdadc_start(void)
{
// start the SDADC_1 by SW trigger
SDADC_1.STKR.R = 0xFFFF;
}
uint32 sdadc1[16];
uint32 sdadc2[16];
void edma_init(void)
{
uint8_t hsr_ch = 48; // this number TBD
// DMA B ch 36 - SDADC0 result ready
// DMA B ch 37 - SDADC1 result ready
// DMA channels for eQADC:
// DMA settings for SDADC_0 request
DMA_B.TCD[36].SADDR.R = (uint32_t)&SDADC_1.CDR.R;
DMA_B.TCD[36].ATTR.B.SMOD = 0; /* source address modulo*/
DMA_B.TCD[36].ATTR.B.SSIZE = 2; /* source data size: 32bit */
DMA_B.TCD[36].ATTR.B.DMOD = 0; /* destination address modulo: 32 datawords each 4 bytes */
DMA_B.TCD[36].ATTR.B.DSIZE = 2; /* destination data size: 32bit */
DMA_B.TCD[36].SOFF.R = 0; /* source address signed offset */
DMA_B.TCD[36].NBYTES.MLNO.R = 32; /* inner "minor" byte count */
DMA_B.TCD[36].SLAST.R = 0; /* TCD Last Source Address Adjustment */
DMA_B.TCD[36].DADDR.R = (vuint32_t)sdadc1; /* destination address */
DMA_B.TCD[36].CITER.ELINKYES.B.ELINK = 0; /* Enable channel-to-channel linking on minor-loop complete */
DMA_B.TCD[36].CITER.ELINKYES.B.LINKCH = hsr_ch; /* Minor Loop Link Channel Number */
DMA_B.TCD[36].CITER.ELINKYES.B.CITER = 4; /* current major iteration count */
DMA_B.TCD[36].DOFF.R = 4; /* signed destination address offset */
DMA_B.TCD[36].DLASTSGA.R = -128; /* last destination address adjustment /scatter gather address */
DMA_B.TCD[36].BITER.ELINKYES.B.ELINK = 0; /* enable channel-to-channel linking on minor loop complete */
DMA_B.TCD[36].BITER.ELINKYES.B.LINKCH = hsr_ch; /* Minor Loop Link Channel Number */
DMA_B.TCD[36].BITER.ELINKYES.B.BITER = 4; /* beginning major iteration count */
DMA_B.TCD[36].CSR.B.MAJORELINK = 1; /* enable channel-to-channel linking on major loop complete */
DMA_B.TCD[36].CSR.B.MAJORLINKCH = hsr_ch; /* Major Loop Link Channel Number */
// DMA settings for SDADC_1 request
DMA_B.TCD[37].SADDR.R = (uint32_t)&SDADC_2.CDR.R;
DMA_B.TCD[37].ATTR.B.SMOD = 0; /* source address modulo*/
DMA_B.TCD[37].ATTR.B.SSIZE = 2; /* source data size: 32bit */
DMA_B.TCD[37].ATTR.B.DMOD = 0; /* destination address modulo: 32 datawords each 4 bytes */
DMA_B.TCD[37].ATTR.B.DSIZE = 2; /* destination data size: 32bit */
DMA_B.TCD[37].SOFF.R = 0; /* source address signed offset */
DMA_B.TCD[37].NBYTES.MLNO.R = 32; /* inner "minor" byte count */
DMA_B.TCD[37].SLAST.R = 0; /* TCD Last Source Address Adjustment */
DMA_B.TCD[37].DADDR.R = (vuint32_t)sdadc2; /* destination address */
DMA_B.TCD[37].CITER.ELINKNO.B.ELINK = 0; /* Disable channel-to-channel linking on minor-loop complete */
DMA_B.TCD[37].CITER.ELINKNO.B.CITER = 4; /* current major iteration count */
DMA_B.TCD[37].DOFF.R = 4; /* signed destination address offset */
DMA_B.TCD[37].DLASTSGA.R = -128; /* last destination address adjustment /scatter gather address */
DMA_B.TCD[37].BITER.ELINKNO.B.ELINK = 0; /* Disable channel-to-channel linking on minor loop complete */
DMA_B.TCD[37].BITER.ELINKNO.B.BITER = 4; /* Beginning major iteration count */
DMA_B.TCD[37].CSR.B.MAJORELINK = 0; /* Disable channel-to-channel linking on major loop complete */
}
void edma_start(void)
{
/* Enable eDMA channels*/
DMA_B.SERQ.R = 36; /* SDADC0 result ready */
DMA_B.SERQ.R = 37; /* SDADC1 result ready */
}
The SDADC_AN[0] connent to 1.25V voltage, the SDADC_AN[1] connect to GND. and the sdadc read back value:
I have change the SDADC_AN[0] to other voltages, but the adc read value was not effect .
Hi,
firstly I would ask whether you have ever SDADC running for instance with simple configuration used in my example here:
Example MPC5777C-SDADC_simple GHS614
I have certain doubts about SDADC configuration, I am missing send key to reset ADC to start sampling, also I guess OSDR would require different values. Is your code based on certain example code?