MPC5775E 3-phase PMSM Development Kit - Power board jumper setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5775E 3-phase PMSM Development Kit - Power board jumper setting

570件の閲覧回数
auftrag2021
Contributor III

Where do these screen shots coming from? Which "quick start guide document" do you mean? I have now serious problem to drive the PMSM. I need very badly the full-document to have a better understanding besides, the jumer setting for the power board is still unclear to me.

Question: Which option shall I supposed to configure? all default?

auftrag2021_0-1648700919448.png

 

0 件の賞賛
返信
1 返信

560件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The quick start guide is the document which is published as and there is nothing more as the web guide is just copied quick start guide. I believe we have supplied this with kit in past. Now it is online.

https://www.nxp.com/document/guide/get-started-with-the-mpc5775e-evb:GS-MCSPTR2A5775E

Which option shall I supposed to configure? all default?

Board is in default setup when is shipped and it can be directly used. User only has to configure JTAG header.

If you dont want SBC chip to reset your device imediately when you connect debugger, you have to remove jumper which connects reset from SBC to the microcontroller.

Otherwise everything should run just fine.

Best regards,

Peter

0 件の賞賛
返信