We are using MPC5748G. The two 16kb HSM data blocks
0x00F80000 to 0x00F83FFF and
0x00F84000 to 0x00F87FFF
are used for NVM data storage.
We have integrated Fls driver from Nxp. With SMPU disabled we are able to read and write to this memory without any problem. But, when we enable SMPU, read/write to this address throws memory protection violation error. We tried to configure a region for above address range in SMPU but still we see the error.
Can you please help?
Hello,
This can be made exclusive to HSM but for parts without HSM programmed this section is available for customers to use as a generic flash partition.
However this section is not advised to be used for on the fly runtime erase/write operations.
refer to errata:
Refer to this EB: EB00875, Considerations for Avoiding Stuck-In-Reset Scenarios Caused by Non-Correctable ECC Errors i...
Could you provide more details here. Like which specific part you are using,etc...
best regards,
Peter
Hi Peter,
Thanks for the reply.
We do not have HSM or in other words, HSM is disabled. We are trying to use the two 16KB HSM data blocks below like a normal Flash section.
0x00F80000 to 0x00F83FFF -> HSM data block0
0x00F84000 to 0x00F87FFF -> HSM data block1
We are trying to store some information in this before shutdown and are reading from this section after bootup.
We are able to read/write without SMPU enabled (SMPU_0 and SMPU_1). When we enable SMPUs we could not read or write to these addresses. We tried providing access to this address range by configuring the region descriptor in SMPU and provided access to all bus masters in MPC5748G, but still not able to read/write.