Hi i need to detect rising edges of a signal but for moments the register counter CNT (eMIOS_1.UC[UCHANNEL_17].CNT.B.CNT) that count to the register A (eMIOS_1.UC[UCHANNEL_17].A.B.A) for moments skips 1 number in the count form 0 to the value wrote in A.
The mode used is "Pulse/Edge Accumulation (continuous)".
I verified this disabling interrupts and only verifying in the main() that the register CNT counts by 1.
For example i have CNT = 0 - 1 - 2 - 3 - ??? - 5.
How is possible?
My code configure:
eMIOS_1.MCR.B.GTBE = OFF;
eMIOS_1.MCR.B.MDIS = 0;
eMIOS_1.MCR.B.FRZ = OFF;
eMIOS_1.MCR.B.ETB = 0;
eMIOS_1.MCR.B.SRV = 0; //Id de servidor
-eMIOS_1
-Channel 17
-Mode "Pulse/Edge Accumulation (continuous)" [MODE=8]
-Bus Counter A [BSL=0]
-1 Edge [EDSEL=0]
-Rising Edge [EDPOL=1]
-Prescaler Divide for 1 [UCPRE=0]
eMIOS_1.MCR.B.GTBE = ON;
I adjunt a 2 simple project verifying that:
Prueba_MPC5746R: It conmute pin PD1 for each 10 counts of PEA.
Prueba2_MPC5746R: Its the same but disable interrupts and verifying that counts bad for each increment of NErrorsI and the two numbers "CNTAuxI2" and "CNTAntAuxI2" are the bad count.
Hi,
how do you read the values? Is your software fast enough to read all values? I have never seen that on my side. Do you have some simple project to reproduce it?
Regards,
Lukas
I adjunt two samples. Prueba2_MPC5746R conmutes for each error count.