MPC5746R eDMA register can't write or read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746R eDMA register can't write or read

1,093 Views
冠军蔡
Contributor I

Dear,

I is  debuging MPC5746R for DMA. But When I use S32DS debug MPC5746R, the DMA register cannot be written or read. The debuger is USB Multilink Universal.

code:

DMA_0.TCD[7].WORD_1.B.SMOD = 0;
DMA_0.TCD[7].WORD_1.B.SSIZE = 0x2; /* 32-bit */
DMA_0.TCD[7].WORD_1.B.DMOD = 0;
DMA_0.TCD[7].WORD_1.B.DSIZE = 0x2; /* 32-bit */
DMA_0.TCD[7].WORD_1.B.SOFF = 0x4; //Source address signed offset
DMA_0.TCD[7].WORD_2.NBYTES.B.NBYTES = 64; /* Minor Byte Transfer Count (16x32-bits)/8=64byte */
DMA_0.TCD[7].WORD_3.B.SLAST = -64;
DMA_0.TCD[7].WORD_4.B.DADDR = (uint32)&DMA_save_result0;
DMA_0.TCD[7].WORD_5.B.CITER_E_LINK = 0; //The channel-to-channel linking is disabled
//DMA_0.TCD[0].WORD_5.B.LINKCH_CITER = 0;
DMA_0.TCD[7].WORD_5.B.CITER = 1;
DMA_0.TCD[7].WORD_5.B.DOFF = 0x4; //Destination address signed offset
DMA_0.TCD[7].WORD_6.B.DLAST_SGA= -64;
DMA_0.TCD[7].WORD_7.B.BITER = 1; //
DMA_0.TCD[7].WORD_7.B.BITER_E_LINK = 0; //0=The channel-to-channel linking is disabled
//DMA_0.TCD[0].WORD_7.B.BITER_BITER_LINKCH = 0;
DMA_0.TCD[7].WORD_7.B.BWC = 0;
DMA_0.TCD[7].WORD_7.B.MAJOR_LINKCH = 1; /* Link to channel 1 */
DMA_0.TCD[7].WORD_7.B.MAJOR_E_LINK = 1; /* Enable channel linking */
DMA_0.TCD[7].WORD_7.B.E_SG = 0;
DMA_0.TCD[7].WORD_7.B.DREQ = 0;
DMA_0.TCD[7].WORD_7.B.INT_HALF = 0;
DMA_0.TCD[7].WORD_7.B.INT_MAJOR = 0;

Error:

MPC574xR Device detected.
Unable to go into background mode.

PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)

I try to access DMA_0 register  other Byte,the result is same.

why can't  access DMA_0 register,i  need  help

    

Kind regards,

CGJ 

0 Kudos
Reply
2 Replies

983 Views
yangbo1
Contributor III

Hi, @冠军蔡 

How do you solve this problem? I encounter a similar problem.

Thanks.

0 Kudos
Reply

1,007 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

The debugger is telling you that in order to change register values, your code cannot run.

Stop the code and then change the values.

Or use debugger which is capable of this operation.

regards,

Peter

0 Kudos
Reply