Hi:
I found there are 2 kinds of input can be configured for MPC5746R PJ[14]: DSPI0 clock input and error input for FCCU. Please see attachment. But i can't find how to distinguish them. Can you help check which register can be set to enable/disable each module? Thanks.
Solved! Go to Solution.
Hi,
This issue is clear now.
The DSPI CLKIN and FCCU ERRIN are both rooted as input without possibility to select or disable one of them.
Therefore when DPSI clock input is on pin PJ[14] user must disable FCCU NCF[60] in FCCU_NCF_E1 register.
However this will still rise fault NCF[60] in FCCU_NCF_S1.
If the user SW validate NCF then NCF[60] must be ignored as it is caused by dual input rooting on PJ[14].
User must select either to have DSPI clk in or FCCU ERRIN functionality on this pin.
Peter
Hi,
This issue is clear now.
The DSPI CLKIN and FCCU ERRIN are both rooted as input without possibility to select or disable one of them.
Therefore when DPSI clock input is on pin PJ[14] user must disable FCCU NCF[60] in FCCU_NCF_E1 register.
However this will still rise fault NCF[60] in FCCU_NCF_S1.
If the user SW validate NCF then NCF[60] must be ignored as it is caused by dual input rooting on PJ[14].
User must select either to have DSPI clk in or FCCU ERRIN functionality on this pin.
Peter
Hi,
They are both connected on input of PJ[14].
Peter
Peter Vlna wrote:
Hi,
They are both connected on input of PJ[14].
Peter
Hi Peter:
Do you mean that the input signal of PJ[14] connect to DSPI and FCCU module simultaneous(seting PAD158 input)? Thanks.
yes,
This is what I expect.
However there can be conflict which I am right now discussing with design.
In scenario where you have PJ[14] selected as input and SPI clock is as input on this pin the FCCU NCF[60] will be set.
On other device (MPC5748G) there is separated IMCR for FCCU[ERRIN] and DSPI. So user can select the input functionality. However here is not this possibility according to IO table.
I will update you when design say they statement.
Peter
Hi Peter:
Any update on this issue? Thanks.
Hi,
No, still no answer from application/design team.
Peter