MPC5746C Boot Assist Flash (BAF)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C Boot Assist Flash (BAF)

1,359 Views
cholland
Contributor V

So, I am starting my foray into figuring out how to get the Boot Assist Flash to work.

Well, from what I understand, if the Boot Header is not found, the BAF will perform a Serial boot.

The Serial boot requires a BAF formatted file.

I figured out how to get the flash driver to work, which allowed me to erase the Boot header.

So, hopefully I am now in Serial boot mode. (Maybe S32 has some way to just erase the flash w/o programming?)

I figured out how to get an srec formatted file out of S32 Design Studio.

I noticed that addresses were not contiguous, so I checked a couple of ticks in S32 Design studio

pastedImage_1.png 

That seemed to make the addresses contiguous.

Next, I chopped it up the .SREC file to leave just the code bytes.

I then added the Password, Load address, VLE bit and program byte length 

as shown below.

/////////  Original SREC Formatted File /////////////

S014000050524A5F4D504335373436422E73726563CD
S31501002C007068E00070E8E0001C6302841CE702843F

....

S70501000000F9

///////// BAF Formatted File /////////////

FEEDFACECAFEBEEF
01000000
8001D3D5
7068E00070E8E0001C6302841CE70284

....

0102431C01

I am using the EVB board, so the external xtal is 80 Mhz, which means I would need 96,000 baud.

I was able to just type in the baud rate on Tera Term VT so hopefully that works.

pastedImage_2.png

I tried sending a file or just sending the password and hope for some echo, but I don't see anything and I am wondering what, if anything, I am doing wrong.

I don't know if anybody else has tried this? I don't see any examples. 

There's not too much discussion of BAF.

Hopefully I am headed in the right direction.

Thanks for your help.

0 Kudos
Reply
2 Replies

1,116 Views
cholland
Contributor V

Peter,

You are correct. I am mistaken. It is indeed 40 MHz.

Other than the xtal, does it look like I am on the right track?

Thanks,

0 Kudos
Reply

1,116 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

are you sure you have 80MHz XTAL?

pastedImage_1.png

Peter