MPC5744P Flexpwm complementary signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P Flexpwm complementary signals

ソリューションへジャンプ
850件の閲覧回数
thomaspham
NXP Employee
NXP Employee

Dear all,

I'm using MPC5744P and trying to make Flexpwm to output PWM45 signal to complementary output pins.

But even when MCTRL[IPOL] bit is set correctly, it is still PWM23 signal chosen.

I'd like to ask if anyone else encountered this problem before?

I found an errata (number 3511) similar to this but in other CPU (MPC567XK) https://www.nxp.com/docs/en/errata/PXS30_0N72D.pdf 

Thank you for reading!

タグ(2)
1 解決策
647件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr

元の投稿で解決策を見る

1 返信
648件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr