MPC5744P Flexpwm complementary signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P Flexpwm complementary signals

Jump to solution
849 Views
thomaspham
NXP Employee
NXP Employee

Dear all,

I'm using MPC5744P and trying to make Flexpwm to output PWM45 signal to complementary output pins.

But even when MCTRL[IPOL] bit is set correctly, it is still PWM23 signal chosen.

I'd like to ask if anyone else encountered this problem before?

I found an errata (number 3511) similar to this but in other CPU (MPC567XK) https://www.nxp.com/docs/en/errata/PXS30_0N72D.pdf 

Thank you for reading!

Tags (2)
1 Solution
646 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr

View solution in original post

1 Reply
647 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr