MPC5744P Flexpwm complementary signals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744P Flexpwm complementary signals

跳至解决方案
772 次查看
thomaspham
NXP Employee
NXP Employee

Dear all,

I'm using MPC5744P and trying to make Flexpwm to output PWM45 signal to complementary output pins.

But even when MCTRL[IPOL] bit is set correctly, it is still PWM23 signal chosen.

I'd like to ask if anyone else encountered this problem before?

I found an errata (number 3511) similar to this but in other CPU (MPC567XK) https://www.nxp.com/docs/en/errata/PXS30_0N72D.pdf 

Thank you for reading!

标记 (2)
1 解答
569 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr

在原帖中查看解决方案

1 回复
570 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Thomas,

This is normally working on the MPC5744P.

The IPOL are buffered bits and do not take effect until a FORCE_OUT event takes place in the appropriate submodule. FORCE_OUT can be generated immediately upon SW FORCE, or based on several other HW signals (local reload/sysnc, master reload/sync, etc).

BR, Petr