Hi,
I come from an FPGA background and am familiar with how FPGA IO bank voltage levels are organized. IO from Bank X has the voltage level that is connected in VCCX. Is there a similar thing for the MPC5676R?
How, by looking at the datasheet, can I figure out the voltage/DC electrical specs for each pin?
In the attached datasheet I see the table in section 4.7 but this doesn't help me as I don't understand which pins are linked to which voltage sources.
And a specific question I have is how do I find the electrical DC specifications for configuration and common uC signals such as the uC RESET?
Thanks,
Nick
If you see MPC5676R Microcontroller Reference Manual,
Table 2-4. Signal Properties and Muxing Summary
All signals have defined it voltage domain (Table 2-4, column Voltage) including system pins as RESET.
Link:
http://cache.nxp.com/files/32bit/doc/ref_manual/MPC5676RRM.pdf
Second question
According to particular voltage in datasheet in section:
Specific RESET specs you may see here: