MPC5674 Internal temperature sensor gone awary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5674 Internal temperature sensor gone awary

869件の閲覧回数
ICStedman
Contributor I

I know there are similar posts but has anyone experienced issues with the internal temperature sensor on the MPC5674 reading too high on recent date codes?

We have experienced issues with devices with dates codes 1634-1707 but the most recent failure was on a date code of 1929. The issue is that the 'calibrated' temperature sensor reads around 15-20C higher than another device, in the same system (at similar ambient). I know it has a +/-10C accuracy but this large a variation has thrown up a few issues here.

0 件の賞賛
7 返答(返信)

750件の閲覧回数
ICStedman
Contributor I

Hi,

The part number is SPC5674FF3MVV3R and the affected date code is 1929.

Previously we have had issues on part SPC5674FF3MVV3R and date codes, 1634-1707

0 件の賞賛

724件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is clear to me.

But I wanted to know whether all 3 devices in the presented table are of the SPC5674FF3MVV3R date code 1929?

Could you share the complete part number (all lines printed on the chip)?

0 件の賞賛

845件の閲覧回数
ICStedman
Contributor I

Awaiting some software expertise to read the calibration constants, then I'll report back. 
Looking at section 33.3 of the MPC5674 reference, for the Temperature formula it has:

Tsens_code(Tlow)=Vtsens(tlow)/Vref0 x 2^14

Below it states, Vref0 is the ADC reference voltage during factory calibration.

Is this a mis-print or is there a Vref0 calibration constant somewhere?

0 件の賞賛

833件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport
0 件の賞賛

857件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

we have no indication there is similar issue with a recent datecodes, but let me check this.
For that, could you please give summary of the values read from TCCR0/TCCR1 registers and ADC reading of temp sensor and bandgap on "bad" part? And comapring this with some OK part if you have.

Thanks,

BR, Petr

0 件の賞賛

805件の閲覧回数
ICStedman
Contributor I

Hi,

Sorry for the delay in replying, has taken some time to get the support needed due to current restrictions.

The data requested:

CardTCCR0TCCR1ThighTlowVbgTsens ADCReported value
GoodA3EA9533CF9EFFFF145-451.22V655916.78C
Suspect 1A17192BACF9EFFFF145-451.23V629636.88C
Suspect 2A3179460CF9EFFFF145-451.22V658226.60C

  

All cards measured on the same rig, within a few minutes of each other. Lab ambient was 23C and 45% humidity. Even the 'good' card is a bit low but I do note the +/-10C accuracy of the sensor.

 

Any suggestions?

0 件の賞賛

784件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, Petr asked me to continue with this thread.

Could you share exact part numbers of this devices including date codes?

0 件の賞賛