MPC565 MODCK pads oscillator set

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC565 MODCK pads oscillator set

757 Views
lucid_lucid86
Contributor I

hi dears

i have designed the board based on MPC565 . and i forgot make pull-up of MODCK signals for set PLL to external Oscillator. and now how can i set it to external Oscillator ?? without pull-up MODCK signals. 

is there any way??? 

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

687 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

by default, there's internal weak pull up resistor on all MODCK pins:

pastedImage_1.png

If nothing else is connected to these pins, this mode should be selected:

pastedImage_2.png

After PORESET is negated the pins can be used as interrupt pins. If the user intends to use these pins as interrupts then it is necessary to ensure that no interrupt signals to these pins are asserted during PORESET. The easiest way to achieve this is to gate any interrupt source to these pins with the /HRESET signal.

Regards,

Lukas

0 Kudos
Reply

687 Views
lucid_lucid86
Contributor I

yes but i need to have 011 set on MODCK pin 

how can i set it?

0 Kudos
Reply