MPC5645S connected to a 18 bit display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5645S connected to a 18 bit display

725 Views
deniszallot
Contributor II

Hello,

I wish to connect the DCU3 (Display Controller Unit) of the MPC5645S to a 18 bit TFT display.

In my opinion, the appropriate way to do that is to connect only the 6 most significant bits of the DCU3 to the LCD panel.

This needs to be done for each of the three colors.

I have not been able to find out which is the most significant bit though.

For the red color,  is it DCU_R0 or DCU_R7?

In other terms, do I have to connect PA0[DCU_R0] to PA5[DCU_R5] or PA7[DCU_R7] to PA2[DCU_R2] to my TFT ?

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

632 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Recommended connection you may find in following appnote, Table 1:

https://www.nxp.com/docs/en/application-note/AN4444.pdf 

pastedImage_4.png