MPC5645S PWM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5645S PWM

1,110 次查看
antonkarzanov
Contributor II

Hello.

Help me please.

Where can I see examples of the source code for setting the static PWM? (PER - const, duty - const)

I tried to configure this module, but they were unsuccessful. The clock modules, timers and GPIO work fine.

Help me please.

/* Fsys = 64 MHz. */

/* init_PWM */

SMC.CTL0.B.DITH = 0;
SMC.CTL0.B.MCPRE = 0x3;
SMC.CTL1.B.MCTOIE = 1;
SMC.CC[2].B.MCOM = SMC.CC[3].B.MCOM = 0x3;
SMC.CC[2].B.CD = SMC.CC[3].B.CD = 00;
SMC.CC[2].B.MCAM = SMC.CC[3].B.MCAM = 0x1;
SMC.PER.B.PER = 100;
SMC.DC[2].B.DUTY = SMC.DC[3].B.DUTY = 50;

标签 (1)
标记 (2)
4 回复数

914 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

we have posted all available example here:

https://community.nxp.com/docs/DOC-329623 

Peter

914 次查看
antonkarzanov
Contributor II

Thanks for the answer.
Which device is closest to the MPC5645S from this list?

Anton.

0 项奖励
回复

914 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

The closest micro is MPC5606S.

But the modules are mostly general trough all MPC microcontrollers.

Unfortunately SMC is not general module and it is implemented only on MPC5606S and MPC5645S.

Peter

914 次查看
antonkarzanov
Contributor II

Ok. Thanks.

0 项奖励
回复