MPC5644A: DSPI_MCR[SMPL_PT] cannot be used with CPHA=1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5644A: DSPI_MCR[SMPL_PT] cannot be used with CPHA=1?

1,097件の閲覧回数
EAlepins
Contributor V

Hi,

 

The MPC5644A RM Rev 6 "Functional description" only talks about SMPL_PT field in the "30.9.6.3 Modified SPI/DSI transfer format (MTFE = 1, CPHA = 0)" chapter, No word about it in "30.9.6.4 Modified SPI/DSI transfer format (MTFE = 1, CPHA = 1)". However, according to its description in the MCR register, it is not tied to any particular CPHA setting.

 

It would be useful for us to delay by 1 or 2 system clocks the sample point of the DSPI SIN (we are in master mode, CPHA=1, CPOL=0). Can we interpreet the Data Setup Time for Inputs (tSUI) of the datasheet (Rev. 7) of 20 ns (for 5V input) as being the time between the SIN data being value and the sample point? If so, then the requirement would become 20 - 2*1/150MHz = 7 ns between data valid and clock rising edge.

 

Thanks,

Étienne

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

811件の閲覧回数
david-mcdaid
NXP Employee
NXP Employee

Hi Étienne,

Unfortunately the relationship between SMPL_PT and CPHA is not detailed in the MPC5644A RM. However I can confirm that the SMPL_PT bit is only valid in the case where MTFE = 1 and CPHA = 0. Here's an excerpt from another device's RM for the same SPI/DSPI module:

dspi_smpl.JPG.jpg

If you wish to use the SMPL_PT delays then you will have to change your CPHA to 0.

I hope this helps!

Thanks,

David

811件の閲覧回数
EAlepins
Contributor V

Thanks. So, with MTFE=1 and CPHA=1, is this field don't care or we have to set it to 0?

Étienne

0 件の賞賛
返信