MPC5644的工程移植MPC5642的芯片

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5644的工程移植MPC5642的芯片

2,289 次查看
jcy
Contributor II

抱歉,英文不太好,可能描述不清楚,麻烦看得懂中文的朋友帮帮忙,万分感谢,

我用CW2.10编写了MPC5644的工程,已经能在MPC5644开发板上成功运行,但是现在想把此工程移植到MPC5642芯片上运行,直接通过CW2.10把工程下载到MPC5642开发板时不能下载成功,下载工程停在了“loading programming algorithm....”,我查到CW2.10没有MPC5642的芯片驱动,就官网下载了最新的CW11.0,通过CW11.0新建了 MPC5642的工程(编写了几行代码验证可以下载到5642的目标板,且能正常运行),然后通过“target tasks”下载CW2.10上生成的MPC5644的*.elf文件,配置如下

1.png

但下载过程中报了如下的错误,

2.png

标签 (1)
5 回复数

1,242 次查看
jcy
Contributor II

problem: The MPC5644 project transplant MPC5642 chip

Peter Vlna, sorry, I'm not good at English. I may not be able to describe it clearly. If you can see it, please help me solve this problem. Thank you very much.I have written in CW2.10 MPC5644 project, already can run successfully on the MPC5644 development board, now I want to transplant the project to run MPC5642 chip, I try to download the project through CW2.10 to MPC5642 development board, but no download success, download process stops at "loading programming algorithm...", before, I don't know CW2.10 not MPC5642 chip driver, it's official website to download the latest CW11.0, through CW11.0 built MPC5642 project (write a few lines of code validation can be downloaded to the 5642 target board, and can run normally), and then through the "target tasks" download on CW2.10 generated MPC5644 the *.elf file, the configuration is as follows

1.png

The following error was reported in the download process

2.png

0 项奖励

1,242 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, this is not Chinese forum. If you require help rewrite your questions in English.

Peter

1,242 次查看
jcy
Contributor II

Hi,Peter Vlna

if you have some good methods about MPC5644a project transplant MPC5642a chip, please give me some advice or experience.Thank you!

0 项奖励

1,242 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I would start with blank project for MPC5642A.

Compiled it, and then start porting drivers from MPC5644A one by one.

Peter

1,242 次查看
jcy
Contributor II

problem: The MPC5644 project transplant MPC5642 chip

Peter Vlna, sorry, I'm not good at English. I may not be able to describe it clearly. If you can see it, please help me solve this problem. Thank you very much.I have written in CW2.10 MPC5644 project, already can run successfully on the MPC5644 development board, now I want to transplant the project to run MPC5642 chip, I try to download the project through CW2.10 to MPC5642 development board, but no download success, download process stops at "loading programming algorithm...", before, I don't know CW2.10 not MPC5642 chip driver, it's official website to download the latest CW11.0, through CW11.0 built MPC5642 project (write a few lines of code validation can be downloaded to the 5642 target board, and can run normally), and then through the "target tasks" download on CW2.10 generated MPC5644 the *.elf file, the configuration is as follows

1.png

The following error was reported in the download process

2.png

0 项奖励