MPC5643L_FlexPWM_question(reload and interrupt)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5643L_FlexPWM_question(reload and interrupt)

2,555 次查看
yanna
Contributor IV
  • Aboout FlexPWM

Q1:   If the VAL1 is required for register reloading and an interrupt, which will happen first, reloading or interrupt?

For example: 

 

FLEXPWM_0.SUB[0].CTRL.B.FULL = 1; // Full cycle reload

FLEXPWM_0.SUB[0].VAL[1].R = 600;     //FLEXPWM0_VAL1; // Max value for counter

FLEXPWM_0.SUB[0].TCTRL.R = 0x1;        //Enable CTU trig only for VAL1

 

      CTU.TGSISR.R = 0x00000800; // active input = PWM_EVEN0 (VAL1 - VAL3 - VAL5 OUT_TRIG1_0 )

      CTU.TGSCR.R  = 0x0000;      //triggered mode

          //Compare modulo & reload value

     CTU.T0CR.R = 0;

     CTU.TGSCRR.R = 0;

     CTU.TGSCCR.R = 1200;

 

//Trigger Handler control registers

     CTU.THCR1.R = 0x00000040;  //T0: enable

     CTU.THCR2.R = 0x00000000;  //T4-T7: disable

 

//Interrupt enable

     CTU.CTUIR.R = 0x0100;//T0 interrupt enable 

 

 

void PWM0_sub0__CTU_T0_Isr(void)

{

    ...

  FLEXPWM_0.SUB[0].VAL[2].R =x;

}

If in the k cycle , the value we read FLEXPWM_0.SUB[0].VAL[2] is 100 and the value currently using

( FLEXPWM_0.SUB[0].VAL[2]) is 200 ,

Case 1: in the k+1 cycle , the value we read FLEXPWM_0.SUB[0].VAL[2] is x and the value currently using( FLEXPWM_0.SUB[0].VAL[2]) is 100;(reload first,interrupt second)

Case 2: in the k+1 cycle , the value we read FLEXPWM_0.SUB[0].VAL[2] is x and the value currently using( FLEXPWM_0.SUB[0].VAL[2]) is x; (interrupt first, reload second)

 

Which case is right?

 

Thanks very much

Yanna

标签 (1)
10 回复数

1,558 次查看
petervlna
NXP TechSupport
NXP TechSupport

Reload happens even if reload interrupt is disabled.

Reload interrupt is an event which can be set on reload.

1,558 次查看
yanna
Contributor IV

Hi,Peter! @Peter Vlna

I still don't know  Reload occur first or Reload interrupt or trigger inturrept first?

Thanks very much!

Yanna

0 项奖励
回复

1,558 次查看
petervlna
NXP TechSupport
NXP TechSupport

1. Reload first

2. Reload interrupt and trigger interrupt in same time.

1,559 次查看
yanna
Contributor IV

Hi,Peter.petervlna

      I think that reload and reload interrupt are different. The loading of the INTI and VALx registers will occur even if the reolad interrupt is disable. Is it right?

       I think my question is about reload and trigger interrupt, but your reply talks about reload interrupt and trigger interrupt, Is it right?

       P685 (MPC5643L reference mannual) ,there exits a sentence:

MPC5643L_mannual_PWM_Reload1.PNG

Thanks very much!

Yanna

0 项奖励
回复

1,559 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

VAL1 determine your PWM period.

If interrupt is set for VAL1 (0x100) then interrupt is triggered when counter reach 0x100.

Register reloading is done when counter resets. (at 0x0)

Peter

1,559 次查看
yanna
Contributor IV

   Q3:

          (1)  If I set the value of the Mask Register 0x0330(PWMA and PWMB output of the submodule 0 and 1 are forced to logic 0), at the same time CTRL2.B.INDEP=0(complentary PWM pair, the submodule 0 and 1)  when a force out signal occur, will the PWMA and PWMB be the logic 0?

          (2)  If OUT23_0=0 and OUT45_0=0(SEL23_0=10, SEL45_0=10, OUT23_0 and OUT45_0 bit is used by the deadtime logic), at the same time CTRL2.B.INDEP=0(complentary PWM pair, the submodule 0)  when a force out signal occur, will both the PWMA and PWMB (the submodule 0) be the logic 0  or  will an error occur ?

Thanks very much!

Yanna

0 项奖励
回复

1,559 次查看
yanna
Contributor IV

Hi,Peter. I have another question about the code above.

  • About CTU

       Q2:  can I set the value of CTU.T0CR(Trigger 0 compare value) same as the CTU.TGSCRR(TGS counter reload value) ? If both

                are equal, will trigger 0 occur? like

      

           CTU.T0CR.R = 0;

      CTU.TGSCRR.R = 0;

           Addition:(That says I want when the count value equal the VAL1 value, trigger 0 (TGS) occur at the same time,

             the ADC command also occur at the same time, delay T0=0 . )

       MPC5643L_mannual_CTU_TGS.PNG

Thanks very much!

Yanna

0 项奖励
回复

1,559 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes you can set trigger to 0. This is its default value after reset.

CTU will trigger when counter reach value 0 -> which is on reload.

Peter

1,559 次查看
yanna
Contributor IV

Hi,Peter. Thanks very much.petervlna

Does It mean that case 2 is right?

Yanna

0 项奖励
回复

1,559 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I did some testing to verify the behavior.

If reload and VAL1 interrupt are set for same timing, first time after enabling of FlexPWM module only reload interrupt will come.

In second and every following period the VAL1 interrupt and reload interrupt are triggered at the same time as the compare is done via hardware. Both interrupt requests are send to INTC module at the same time.

If in INTC the priority for VAL1 and reload interrupts are same then reload interrupt is served first (as its number in interrupt table is lower) and then VAL1 interrupt is served.

If you set priority for those interrupts then interrupt with higher priority is called first.

pastedImage_0.png

Peter