Dear NXP supporter:
The development enviroment is: S32 DS V2.1, P&E mutliLink universal debugger
Brief description of my issue is:
A MPC5642A project with PIT ISR, can't run at full speed in deugging mode, it can only be single step executed.
The very simple project (name: mpc5642_test-noISR) created with S32 DS Wizard, it can be flashed into ECU and debug with P&E multiLink at full speed.
Simple project is created like below:
I downloaded a PIT ISR example (name: MPC5644A_ISR, on MPC5644A) from NXP website, and ported it to the MPC5642A project (project name: mpc5642_test-withISR)
For the project mpc5642_test-withISR, the issue:
during debugging, I pressed the 'resume(F8)' button, the code run one step, then stopped automatically.
For example: the cursor stopped at entry position (the '{') of ISR pit0_hanlder(). please refer to following snapshot
Then I press the resume button, it then stopped at exit position (the '}') of ISR pit0_handler()
Could you please give me some hint? thank you in advance.
BR
Zhou YiChuan
Following is the screen snapshot while debuggijng.
已解决! 转到解答。
Hi,
there are several ways how to write nop:
__asm__("nop");
__asm__("e_nop");
__asm__("se_nop");
The first one should be used when using BOOK E instruction set. Next ones when using VLE set.
Your project is VLE. If you use
__asm__("nop");
... it is translated as:
se_bclri r0,0x0
se_illegal
If a debugger is connected, se_illegal works as a software breakpoint.
So, solution is to use VLE versions:
__asm__("e_nop");
__asm__("se_nop");
In CodeWarrior IDE, __asm__("nop"); was automatically translated to VLE instruction set. But the situation is different in S32DS and you need to use VLE versions explicitly.
Regards,
Lukas
Hi,
there are several ways how to write nop:
__asm__("nop");
__asm__("e_nop");
__asm__("se_nop");
The first one should be used when using BOOK E instruction set. Next ones when using VLE set.
Your project is VLE. If you use
__asm__("nop");
... it is translated as:
se_bclri r0,0x0
se_illegal
If a debugger is connected, se_illegal works as a software breakpoint.
So, solution is to use VLE versions:
__asm__("e_nop");
__asm__("se_nop");
In CodeWarrior IDE, __asm__("nop"); was automatically translated to VLE instruction set. But the situation is different in S32DS and you need to use VLE versions explicitly.
Regards,
Lukas