MPC5606BK  enter low power and wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5606BK  enter low power and wake up

1,220 Views
458362783
Contributor I

hello All

      I'm going to use low power module, but I don't know how to configure it. Who can provide me an example?

 

 

low power module  ( I want MPC5606BK enter STOP mode  and    then wake up  from  I/O    )

 

thanks

Labels (1)
0 Kudos
Reply
2 Replies

843 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are examples for low power mode in this application note:

http://www.nxp.com/files/32bit/doc/app_note/AN2865.pdf

http://www.nxp.com/webapp/sps/download/license.jsp?colCode=AN2865SW

You can also use this example:

https://community.nxp.com/docs/DOC-100206

It enters STOP mode and it wakes up on edge on WKUP pin. Just do not enable the CAN sampler.

Regards,

Lukas

0 Kudos
Reply

842 Views
458362783
Contributor I

HI,Lukas!

Thank you very much!  

With the help of you, I can into the lower power stopped mode.  According to the following code:

ME.STOP0.B.PDO = 1; /* Pad power sequence driver disabled, */
/* but state of the output is kept */
ME.STOP0.B.MVRON = 0; /* Main Voltage regulator is off */
ME.STOP0.B.DFLAON = 1; /*Data flash is in power-down mode */
ME.STOP0.B.CFLAON = 1; /* Code flash is in power-down mode */
ME.STOP0.B.FMPLLON = 0; /* FMPLL off (default status during STOP) */
ME.STOP0.B.FIRCON = 0; /* Fast internal RC oscillator off */
ME.STOP0.B.FXOSC0ON = 0;/* Fast external crystal oscillator off */


ME.STOP0.B.SYSCLK = 0x0f; /* System clock is disabled */


ME.STOP0.B.PDO = 1; /* Pad power sequence driver disabled, */
ME.MCTL.R = 0xA0005AF0; /* Enter STOP Mode & Key */ 
ME.MCTL.R = 0xA000A50F; /* Enter STOP Mode & Inverted Key */

if   ME.STOP0.B.SYSCLK = 0x0f;         the low power current is 2.96ma  ,  but  I cannot wake up  MCU by  wakeup[4]

if   ME.STOP0.B.SYSCLK = 0x02(or 0x02);         the low power current is 16ma  ,  and  I can wake up  MCU by  wakeup[4]

Now, I need  the low power current <5ma.How can I to Configure the above code section.

0 Kudos
Reply