What are the differences between MPC5604B_M07N and MPC5604B_M27V derivatives?
I have XPC560B 100LQFP and XPC560B 144LQFP. At the begining I was working with 144 ( I was using MPC5604B_M27V MCU in CW project wizard, but I don't now why...) but now I need to work with 100, and I don't know if I need change that.
Thank you.
I received this explanation from Freescale support:
"...
The difference is in mask set and their errata. But the mask 07N has never been produced so you can omit this option. I will inform CodeWarrior to remove it.
You should select mask set M27V and everything will be OK.
The mask set defines internal circuitry => errata list. It has no influence on defined features defined by reference manual and data sheet...."