MPC5575B SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5575B SDK

跳至解决方案
1,698 次查看
TerryDuPower
Contributor III

Dear Supporter:

     How to download and install MPC5575B SDK?

     I can't find MPC5575B SDK after I install the S32 design studio for Power architecture.

     I get an error when I open a project, seems missing MPC5575B SDK.

TerryDuPower_0-1643274104341.png

BestRegards!

Thanks!

标记 (1)
0 项奖励
回复
1 解答
1,684 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

SDK is installed into c:\NXP\S32DS_Power_v2.1\S32DS\software\ folder. You can check if you have it there

PetrS_0-1643368455435.png

It is installed online via S32DS Extensions and Updates, but also offline option is available
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-S32-Design-Studio/ta-p/11... 

BR, Petr

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,697 次查看
TerryDuPower
Contributor III

sorry, I spell error.  

It should be MPC5775B SDK    not MPC5575B SDK.

0 项奖励
回复
1,685 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

SDK is installed into c:\NXP\S32DS_Power_v2.1\S32DS\software\ folder. You can check if you have it there

PetrS_0-1643368455435.png

It is installed online via S32DS Extensions and Updates, but also offline option is available
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-S32-Design-Studio/ta-p/11... 

BR, Petr

 

0 项奖励
回复
1,673 次查看
TerryDuPower
Contributor III

Hi Petr,

Thanks very much!

BestRards!

 

 

0 项奖励
回复