MPC5575B SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5575B SDK

Jump to solution
1,631 Views
TerryDuPower
Contributor III

Dear Supporter:

     How to download and install MPC5575B SDK?

     I can't find MPC5575B SDK after I install the S32 design studio for Power architecture.

     I get an error when I open a project, seems missing MPC5575B SDK.

TerryDuPower_0-1643274104341.png

BestRegards!

Thanks!

Tags (1)
0 Kudos
Reply
1 Solution
1,617 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

SDK is installed into c:\NXP\S32DS_Power_v2.1\S32DS\software\ folder. You can check if you have it there

PetrS_0-1643368455435.png

It is installed online via S32DS Extensions and Updates, but also offline option is available
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-S32-Design-Studio/ta-p/11... 

BR, Petr

 

View solution in original post

0 Kudos
Reply
3 Replies
1,630 Views
TerryDuPower
Contributor III

sorry, I spell error.  

It should be MPC5775B SDK    not MPC5575B SDK.

0 Kudos
Reply
1,618 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

SDK is installed into c:\NXP\S32DS_Power_v2.1\S32DS\software\ folder. You can check if you have it there

PetrS_0-1643368455435.png

It is installed online via S32DS Extensions and Updates, but also offline option is available
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-S32-Design-Studio/ta-p/11... 

BR, Petr

 

0 Kudos
Reply
1,606 Views
TerryDuPower
Contributor III

Hi Petr,

Thanks very much!

BestRards!

 

 

0 Kudos
Reply