MPC5554 EBI Bus Collision on Transaction Acknowledge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5554 EBI Bus Collision on Transaction Acknowledge

730件の閲覧回数
misrahimmorales
Contributor I

Does the EBI bus have any internal timeout capability if it is unable to drive the Transaction Acknowledge signal low during a Chip Select access because of another Master driving Transaction Acknowledge inactive incorrectly? 

 

I am trying to understand the fault that can occur if the above scenario occurs.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

659件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is an EBI bus monitor, pay attention to

12.3.1.5 EBI Bus Monitor Control Register (EBI_BMCR)

If enabled bus monitor expiration leads in bus error exception.

0 件の賞賛
返信