MPC555 3V I/O Drive Strength

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC555 3V I/O Drive Strength

跳至解决方案
840 次查看
mohammak
Contributor II

Looking at MPC555 / MPC556 datasheet for I/O drive strength in page 64, a strength of 25/50pF is mentioned for 3V pins.

This is confusing because I cant confirm whether 25pF strength is for MPC555 and 50pF strength is for MPC556,

OR

25pF is half strength and 50pF is full strength for both MPC555/MPC556,

Can you please explain.

Thanks

0 项奖励
1 解答
828 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas

在原帖中查看解决方案

1 回复
829 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas