MPC5125 Replace DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5125 Replace DDR

Jump to solution
1,333 Views
zhangbin_eos
Contributor III

I want to replace the DDR of mpc5125 from 256MB to 512MB,
The hardware has replaced 512MB DDR, which is pin compatible. Without modifying the code, the kernel can start normally, but the DDR displayed is 256MB,
What parts do I need to change to enable the kernel to apply larger DDR?
Do you have any relevant documents or examples for reference?

Tags (2)
0 Kudos
1 Solution
1,307 Views
Pavel
NXP Employee
NXP Employee

Change DDR setting in u-boot configuration file and rebuild u-boot. Find .h file for the MPC5125 board using the following path in u-boot source folder:

/include/config

 

Attached file contains this file for the ads5125 board.

View solution in original post

0 Kudos
1 Reply
1,308 Views
Pavel
NXP Employee
NXP Employee

Change DDR setting in u-boot configuration file and rebuild u-boot. Find .h file for the MPC5125 board using the following path in u-boot source folder:

/include/config

 

Attached file contains this file for the ads5125 board.

0 Kudos