MC33907 and trace32 usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33907 and trace32 usage

1,433件の閲覧回数
manuelaielo
Contributor II

Hello,
I'm using a MPC5643L connected to MC33907 as SBC.

Is there any way to flash the code via lauterbach trace32 in Normal mode (no Debug mode activate)?

 

Thank you in advance

Best Regards,

Manuela

ラベル(1)
タグ(4)
4 返答(返信)

1,269件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's no direct support for this in Lauterbach debugger. You have to write a script which will initialize the MCU, configure the SPI and disable the watchdog via SPI. The default timeout of watchdog is 256ms, so the script must be faster...

Regards,

Lukas

1,269件の閲覧回数
manuelaielo
Contributor II

Hi Lukas,

thanks for your answer. I need some more details.

For disable the WDT do you mean set the WDT window to disable?

256ms is the timeout to feed the first time the WDT, in the code I tried to disable the WDT without serving it, but the results was a reset. So is it possible do it?

Regards,

Manuela

0 件の賞賛
返信

1,269件の閲覧回数
rweiss
Contributor V

Hi Manuela,

yes, you have to set the WDT window to disable. In order to get everything done in time, you have to use the Data.STARTUP commands. With Data.STARTUP.SEQuence you can define which values should be written to which address immediately after SYStem.Up or after Power-on (using SYStem.Mode.StandBy). You have to do everything    needed to send the required SPI commands to the SBC, i.e. ME_ME, SIUL, and DSPI. to If I understand the manual correctly, the 256ms configuration time is only available after power-on, so you have to use Data.STARTUP in combination with SYStem.Mode.StandBy. Here is a templace for the setup script:

;turn off target power

SYStem.CPU MPC5643L

;set up Data.STARTUP to send the SPI commands

Data.STARTUP.SEQuence SET <addr> %<width> <value> SET <addr> %<width> <value> ....

Data.STARTUP.ON

;set up StandBy mode to connect and halt core at power-on

Break.Set 0--0xFFFFFFFF /Program /Onchip

SYStem.Mode.StandBy

;turn on target power

If everything worked well, the core should be halted at the reset address now.

See general_ref_d.pdf for details on how to use Data.STARTUP.

Best regards,

Reinhard

1,269件の閲覧回数
manuelaielo
Contributor II

Thank you very much,

Best Regards,

Manuela

0 件の賞賛
返信