Low voltage detection for MPC5775B/E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low voltage detection for MPC5775B/E

772件の閲覧回数
Baris
Contributor II

Can anyone help with low voltage detection for MPC5775B?
I need a sample code.

Screenshot_1.png

Screenshot_2.png

  I wrote a code like this, but it doesn't work, what am I doing wrong?

タグ(2)
3 返答(返信)

705件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

How do you test it? This sequence seems to be correct.

0 件の賞賛
返信

702件の閲覧回数
Baris
Contributor II

Firstly, at what voltage range does LVD operate? Is it 5V, 1.2V, or 3.3V?

Secondly, the VLD_ISR function shown in the images I provided never seems to work. When we cut off the power to the board by connecting an oscilloscope probe to the PTF pin, we didn't see any voltage fluctuations on the PTF pin.

 

0 件の賞賛
返信

646件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you would cut the power, this would not cause LVD issue, but POR. What you enabling, it is core voltage LVD event, that is 1.2V supply rail. This could happen in case attached external 1.2 voltage goes below LVD limits what normally does not happen when core voltage is internally regulated.

davidtosenovjan_0-1676886045046.png

 

0 件の賞賛
返信