Low voltage detection for MPC5775B/E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Low voltage detection for MPC5775B/E

818 Views
Baris
Contributor II

Can anyone help with low voltage detection for MPC5775B?
I need a sample code.

Screenshot_1.png

Screenshot_2.png

  I wrote a code like this, but it doesn't work, what am I doing wrong?

Tags (2)
3 Replies

751 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

How do you test it? This sequence seems to be correct.

0 Kudos
Reply

748 Views
Baris
Contributor II

Firstly, at what voltage range does LVD operate? Is it 5V, 1.2V, or 3.3V?

Secondly, the VLD_ISR function shown in the images I provided never seems to work. When we cut off the power to the board by connecting an oscilloscope probe to the PTF pin, we didn't see any voltage fluctuations on the PTF pin.

 

0 Kudos
Reply

692 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you would cut the power, this would not cause LVD issue, but POR. What you enabling, it is core voltage LVD event, that is 1.2V supply rail. This could happen in case attached external 1.2 voltage goes below LVD limits what normally does not happen when core voltage is internally regulated.

davidtosenovjan_0-1676886045046.png

 

0 Kudos
Reply