gmemfile: warning: hole of size 0x6ffe4 between.rcw ending at 0xf9001c and.vletext starting at 0x1000000
what does this warning means?and how to Eliminate the warning ?
Thanks!
Hi
Which part are you using? Which compiler are you using?
The general answer would be:
If the address space is continuous you can create just one memory section instead of separate blocks
e.g. default MPC5744P linker script file for GCC from project generated by S32DS:
MEMORY
{
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0004, len = 0x4
m_text : org = 0x1000000, len = 2048K
m_data : org = 0x40000000, len = 384K
local_dmem : org = 0x50800000, len = 64K
}
in the linker script above there is a gap 0x00FA0008..0x00FFFFFF
to avoid the gap you can adjust the m_text block:
MEMORY
{
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0004, len = 0x4
m_text : org = 0x00FA0008, len = 2432K - 8
Hope it helps.
Stan