Is there any using method about mpc5748(0N78S/1N81M)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any using method about mpc5748(0N78S/1N81M)?

1,020 Views
seokwonkim
Contributor I

I use mpc5748 with X-MPC574XG-324DS, TRACE32.

When I used PPC5748GMMN6A / 1N81M, there was no problem for using this microcontroller.

But when I change the microcontroller to PPC5748GSMMN6 / 0N78S, TRACE32 cannot detect this microcontroller.

So I want to know if there is a different method using these two chips.

Thank you.

0 Kudos
Reply
4 Replies

813 Views
rweiss
Contributor V

What error messages do you get? Check the AREA window (Menu: View - Message Area).

Best regards,

Reinhard

0 Kudos
Reply

813 Views
seokwonkim
Contributor I

In message area I can see this message

JTAGID=0x0988201D
Processor with JTAGID 0x0988201D not supported by this debugger software version.
Get the latest software update from http://www.lauterbach.com/update.html and
try again. If the problem persists, contact support@lauterbach.com to request
a software update for your device.
debug hardware configuration error

Thank you

0 Kudos
Reply

813 Views
rweiss
Contributor V

Follow the instructions in the message: Install the latest software update.

Best regards,

Reinhard

0 Kudos
Reply

813 Views
seokwonkim
Contributor I

Thank you so much for your effort.

I solved my problem with your help:smileyhappy:

0 Kudos
Reply