Inquiries about Flash ECC Test for MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Inquiries about Flash ECC Test for MPC5777C

266 次查看
youngseolee
Contributor III

Dear NXP Engineers,

I am checking the 1 or 2 bit ECC error detection function by referring to the application note(Error Correction Codes Implemented on MPC5777C or MPC5775B/E) you provided.

Regarding that, I have two questions.

1. If adress 0x00400060 is read, an interrupt is generated by the 2-bit Error Detection condition, but if adress  0x00400040 is read, an interrupt is not generated by the 1-bit Error Correction condition.
In the application note, there are no other conditions other than the Read of 0x00400040 area to inject 1 bit error. Is an additional procedure required for 1-bit error injection?

2. After injection of 2-bit error detection, it seems that exception handlers are continuously generated when the CPU reads FCCU-related registers. If this is a normal operation, what should I do to stop exception handler from occurring continuously?

I look forward to your reply.

thank you

0 项奖励
1 回复

257 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) Single-bit error reporting needs to be enabled by SBCE bit. It is stated in section 9.3 of mentioned document.

davidtosenovjan_0-1668612254659.png

2) I need to add FCCU chapter, as these examples codes does not use FCCU at all, it is also option. If FCCU is used, it is needed to handle FCCU alarm/fault as well. At this moment I would recommend to see following appnotes, where using of FCCU is described:

Using FCCU on MPC5744P:

https://www.nxp.com/docs/en/application-note/AN5284.pdf

and

Error Correction Codes Implemented on MPC5744P:

https://www.nxp.com/docs/en/application-note/AN13179.pdf

 

 

 

0 项奖励